RomanSolonto Posted January 17, 2017 Share Posted January 17, 2017 I do not see any servo channels in "System setup" of Power Pmac IDE. I have last versions of Power Clipper firmware and IDE. What can I do to solve this problem? Thank you Link to comment Share on other sites More sharing options...
steve.milici Posted January 25, 2017 Share Posted January 25, 2017 System setup functions for the Power Clipper are currently under development. At this time use the setup code provided in the "Power PMAC Clipper User Manual" on the Forums' FileDepot: "http://forums.deltatau.com/filedepot/download.php?f=Power PMAC/Manuals/Hardware Reference Manual/Power PMAC Clipper User Manual.pdf" Link to comment Share on other sites More sharing options...
RomanSolonto Posted January 29, 2017 Author Share Posted January 29, 2017 Thank you. But there is one strange thing. In other Power Clipper ( it was "one of the original Power Clippers" http://forums.deltatau.com/showthread.php?tid=2323) it worked at the same versions of the firmware. Now I can't use alias "Clipper[0]", only "Gate3[0]". Is it normal? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted January 30, 2017 Share Posted January 30, 2017 There was a glitch in the Gate ID programming system. Unfortunately this board will need to be sent back for re-programming. If you do not want to do this you can continue using Gate3 in lieu of Clipper without issue. Link to comment Share on other sites More sharing options...
steve.milici Posted January 30, 2017 Share Posted January 30, 2017 This is not normal. What is the barcode serial number of this card? Also what is the response of the following: Gate3[0].PartNum Gate3[0].PartOpt0 Gate3[0].PartRev Gate3[0].PartType Link to comment Share on other sites More sharing options...
steve.milici Posted January 30, 2017 Share Posted January 30, 2017 Note that it may be possible to field reprogram the unit depending on the response from my previous post. Link to comment Share on other sites More sharing options...
RomanSolonto Posted January 31, 2017 Author Share Posted January 31, 2017 I have 2 Clippers. The problems are simmilar. first: Gate3[0].PartType 618089 Gate3[0].PartOpt0 $ffffffff Gate3[0].PartRev 15 Gate3[0].PartType 15 barcode C000FR2A second: Gate3[0].PartType 618089 Gate3[0].PartOpt0 $ffffffff Gate3[0].PartRev 15 Gate3[0].PartType 15 barcode C000GJ2Z Link to comment Share on other sites More sharing options...
steve.milici Posted January 31, 2017 Share Posted January 31, 2017 This is now a technical support issue. Please send an email to support@deltatau.com with this information. I will have our quality group correct this right away. We can then email you corrective reprogramming instructions. Link to comment Share on other sites More sharing options...
CVillaleiva Posted December 12, 2017 Share Posted December 12, 2017 Hi, i have the same problem, and when ask for the information , the PMAC response: Gate3[0].PartType 0 Gate3[0].PartOpt0 nan Gate3[0].PartRev nan Gate3[0].PartType nan and if answer with Clipper[0] Clipper[0].PartType nan Clipper[0].PartOpt0 nan Clipper[0].PartRev nan Clipper[0].PartType nan ------------ for the motor setup, i create a .cfg file in the configuration folder and put the setup code, but when i ask for some configuration variable the value are different that i setup in the file. Link to comment Share on other sites More sharing options...
Recommended Posts