[/b][/size]Dear Sir
I am using TURBO PMAC PCI Lite with analog DAC signals.
i want to isolate analog circut isolation/input flag supply/AENA supply control. Currently i am taking all supplies from pc bus.
i want to isolate
1) INPUT FLAG SUPPLY CONTROL:-If E90 connects pins 1 and 2 and E89 is OFF, the input flags are supplied from a separate A+V supply through pin 9 of the J9 JEQU connector.
IS IT OK???
2) AENA/EQU Supply Control :If E100 connects pins 2 and 3, the circuits will be supplied from a separate A+V supply brought in on pin 9 of the J9 JEQU connector.
IS IT OK???
3) Analog Circuit Isolation Control
E85, E87, E88 are off and The positive supply (+12 to +15V) should be brought in on the A+15V line on pin 59. The negative supply (-12 to -15V) should be brought in on the A-15V line on pin 60. The analog common should be brought in on the AGND line on pin 58.
please confirm whether it is ok as in diagram on page 5 in manual it is showing J7 connector and J9 is connected ie connection under j9 is showing crossing only.please check and confirm.
regards
rajkumar attri
rajkumar.attri@aisglass.com