Omron Forums Support
Omron-
Posts
0 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by Omron Forums Support
-
NERLITE currently does not offer a SCDI-25 that uses blue LEDs. If you require a blue SCDI then you would need to use: P/N: NER-010304020 SCDI-50 V2, B LED-D, 12V-C, 6 ft. Cbl w/ DB9
-
Before executing the attached WSF File (Windows Script File), you must: - Certify that Telnet Client is enabled on Windows. For more information, please check the article "Enabling Telnet Client on Windows". Attention: This simple package does not check the entered values and does not check if the Dual Boot is installed on the unit! When executed: 1. Enter the MicroHAWK IP Address and click OK. 2. Select the Boot Package Option and the Boot Package Number. 3. Click OK. The ‘lbp’ command is executed. 4. At the "Thank you" message, click OK to close the command screen. Operating System Any
-
This article is a step by step guide for settings up Microhawk smart camera to send FTP images. It shows how to setup the server side using Filezilla, as well as disable firewall. Please see attached document for a step by step guide on reader setup (=client) and server setup.
-
Telnet to the device IP Address (For ID/MV 30: 192.168.188.2) and Login using VxWorks login : target Password ; password (You will not see the password Echoed on the screen) then at the prompt "->" issue the command: sysConsolePortHelp() + Enter To end your Telnet session at the prompt "->" issue the command: reset. + Enter When you see "Connection to Host Lost" you can then close the window. Operating System Any
-
HS-1 Stand 98-000108-01 HS-2D and Mobile Hawk stand 98-000153-01 Contact your Microscan distributor for Pricing.
-
In September 2008, Microscan acquired the Siemens Machine Vision group, which through the mergers over the years can be traced back to Itran. Itran is the company developed the MVP 2000T (I-Pak Classic) vision system. In 1999, RVSI Acuity CiMatrix notified all registered I-Pak Classic customers that product support could only be guaranteed through December 2000. At this point Microscan does not provide support for the I-Pak Classic vision system. Microscan has expanded on the capabilities of the I-Pak Classic vision system over several generations of product and currently offers the Visionscape I-Pak vision system to meet the pharmaceutical packaging inspection requirements. More information on this product can be found on the Microscan website at: http://www.microscan.com/en-us/Products/Engineered-Solutions/I-PAK-Package-Inspection-System.aspx This web page provides a brief overview of the Visionscape I-Pak models that are currently offered and provides a link to the current I-Pak spec sheet.
-
The Area Arrays with diffusers are no longer available. This is because they were replaced by the Backlight BL series, which will provide more even illumination. To replace the Diffused AR currently used, select the backlight with the same color and similar size, when compared to the AR model.
-
Here is the procedure to reset the Ethernet card: Note: Restoring the Ethernet card to its factory default settings will clear all current settings except the IP address settings and the administrator password. 1. Power off the scanner. 2. Separate the MS-890 from the wiring box using the four screws in the corners. 3. Locate the reset switch between P3 and CR1 on the Ethernet card. 3. Power on the scanner while holding the reset switch down. (Hold it down for about 20 seconds.)
-
The attached white paper is about using Telnet to reset a Vision MINI or Vision HAWK ConsoleTTY for use with AutoVISION and Visionscape. kA23800000008KYCAY_en_US_1.pdf
-
If scanning the RIMS barcode, but file is not found: Insure the QC or LVS7000 PC is turned ON. RIMS can only retrieve job data from a powered PC. Insure the QC / LVS7000 PC is on the Network. This may require customer IT support. Insure the JOBS folder on the In1= PATH (QC / LVS7000 PC) has File Sharing enabled. This may require customer IT support. [Rims] A5Follows=4 Debug=0 EncoderDirection=0 EncoderPort=5 HomeToPhotoeye=12 In1=\\Server1\PathToJobsDir In2=\\Server2\PathToJobsDir In3=\\Server3\PathToJobsDir Out=\\ServerX\PathToJobsDir LinesPerInch=400 MoveBarcodeInches=0 RewinderOffset=41500 StopDwellInMs=20 Turret=0 Insure the RIM system currently logged in Windows User has permissions to the shared file folders within QC / LVS7000. This also may require customer IT support. Software Version All Firmware Version All Operating System Windows 7
-
A common request is to convert RS-232 serial data to USB HID Keyboard input. The attached spec sheet is for an adapter that seems to work well as a USB Keyboard input device. The DB-9 connector will plug into any Microscan RS-232 Host cable with DB-9 termination. When using the keyboard interface, keep in mind: - All data coming from the device will be typed into any active window. this interface should not be used in automated applications. - keyboard throughput is slower than other interfaces, so it should not be used in high speed applications. kA23800000008J0CAI_en_US_1.pdf
-
Attached Symbols for Testing: Operating System Any
-
The pinouts of all connecotrs on auto ID readers can be found in the appendix of the User's Manual, under electrical specifications. User's Manuals can be downloaded here: http://www.microscan.com/en-us/ServiceAndSupport/DownloadCenter.aspx
-
The LVS-9570 operator manual describes the proper technique for verifying a barcode when using LVS-9570. The unit should be pulled at a slow, steady rate toward the user in the direction toward the back of the unit (where the USB connector is located). This is in the opposite direction of the arrow printed on the outside of the housing, which is used to indicate where the center of the scanning sensor is located. If the LVS-9570 is pulled too quickly across the label, then an over-speed error will be displayed in the LVS-95XX software and no grade will be provided. Barcodes of up to 305 mm (12") long can be scanned in a ladder orientation, with a maximum 137mm (5.4") maximum barcode height. Operating System Windows 10;Windows 7
-
In AutoVISION 4.0+, connect to the camera and take control (lock) press CTRL-SHIFT-L The License Manager window will open to allow you remove the license from the camera, as seen below. ** DO NOT REMOVE the Machine Vision.lic ** To restore, go to license folder and rename the desired license back to *.lic
-
This cable is not supported by Microscan. To order a replacement, contact Brent at NTS ntsbrent@comcast.net
-
QX-870 flying leads cordsets, where to use each?
Omron Forums Support posted a topic in Code Reading
61-000166-01: Connector B (serial) 61-000167-01: Connector A and P/M -
The attached file will show a simplified schematic of the input circuit to the QX-870. This diagram will show the electrical connections of Trigger, New Master, and Input 1 on connectors A, B and T. The diagram also shows the Standard trigger sensors (99-000020-xx, 99-000017-xx) wired into the circuit. The intent of this diagram is to help you understand how to wire the inputs for your application. Pay special attention to the wiring of the trigger, Notice that the Input Common line is toggled to control the read cycle. This is necessary in order for the QX-870 to pass the signal to other readers through connectors A and B. When the circuit is wired in this fashion, the New Master pin and Input 1 can not be used. To use The New Master pin, or to use input 1, you must re-wire the trigger sensor so that Input common is tied to Power, and the NPN trigger signal feeds into the Trigger2 line. When wired in the fashion, the trigger signal will not feed to other readers through connectors A and B. Common problems when wired incorrectly: Using the New Master pin triggers the reader Two readers triggered by one sensor when the trigger lines are not connected (the input common line may be tied together to cause this). Trigger input does not work. New Master pin does not work. New Master pin operation is intermittent.
-
With a Change to Implicit Messaging the below .EDS files are the new form of setup. kA23800000008JcCAI_en_US_1.zip
-
QX Hawk Daisy Chain Setup Setup Secondary QX Hawk cameras first Read Cycle > Trigger = Serial Data Read Cycle > End of Read Cycle > Mode = Timeout Read Cycle > End of Read Cycle > Read Cycle Timeout = 20ms less than previous camera in daisy chain Symbologies > Data Matrix > ECC 200 = Disabled Symbologies > Code 39 = Disabled Symbologies > UPC/EAN = Enabled Calibrate camera (or set Gain, Shutter, & Focus values) Send and Save to camera (<Z>) Confirm proper reading via serial trigger (<space>) < > Repeat for each secondary camera in daisy chain Setup Primary QX Hawk Camera (if desired) Comm > Array Comm > Daisy Chain ID Status = Enabled (Shows which camera read the code) Read Cycle > Trigger = Serial Data Read Cycle > End of Read Cycle > Mode = Timeout Read Cycle > End of Read Cycle > Read Cycle Timeout = max time per application Symbologies > Data Matrix > ECC 200 = Disabled Symbologies > Code 39 = Disabled Symbologies > UPC/EAN = Enabled I/O – Set desired Output configuration (Symbol Data Output, Output 1,2,3 parameters) Matchcode > Matchcode Type = Enabled (if desired) Matchcode > Mismatch Replace = Enabled Utilities > Master Database > enter desired match string Calibrate camera (or set Gain, Shutter, & Focus values) Send and Save to camera (<Z>) Confirm proper reading via serial trigger (<space>) < > In Terminal enter the following command <K150DAISY> You should see a response like: <DAISYCHAIN: Slaves = 1><DAISYCHAIN: Units Resetting><DAISYCHAIN: setup complete><DAISYCHAIN: resetting master unit> Cycle power to the cameras. Otherwise the camera may not respond to triggers properly. Connect to the Primary unit again and change Read Cycle > Trigger = External Edge Send and Save to camera (<Z>) When the <K150DAISY> is executed, the trigger mode on the secondary camera change to match the primary. By executing the <K150DAISY> when the trigger = Serial Data, the secondary units will only respond to a serial trigger to start the read cycle. If the primary camera has the trigger = External Edge, then after the <K150DAISY> all of the secondary cameras will be responding to the external trigger as well. This did appear to work in the limited testing in the office. MD – 2017-02-07 Operating System Any
-
This problem typically occurs when trying to run FrontRunner or AppRunner software. An error: R6030 CRT not initialized message, which causes FrontRunner or AppRunner to immediately terminate. The source of the problem is a conflict with a National Instruments software component that is installed on the computer. The offending component is often located in C:\Program Files\National Instruments\Shared\mDNSResponder\nimdnsNSP.dll renaming this from .dll to .sav corrects the problem with Visionscape software and allows FrontRunner or AppRunner to start properly.