Machine Vision
243 topics in this forum
-
- 0 replies
- 264 views
The version of firmware installed in the VS-1 MUST match the version of Visionscape installed. If the versions do not match, visionscape and the VS-1 will become unstable.
Last reply by Omron Forums Support, -
- 0 replies
- 306 views
The MS-2 is not a drop in replacement. We have created this solution to show the most significant differences when discussing the MS-2 as a replacement. kA23800000008EMCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 289 views
In a Visionscape GigE system the digital I/O is mapped to Virtual I/O starting with Input 1 being mapped to Virtual 161. If 16in/16out board is used, - Inputs start at Virtual 161 to 176 - Outputs start at Virtual 177 to 192 If 32in/32out board is used, - Inputs start at Virtual 161 to 192 - Outputs start at Virtual 193 to 224
Last reply by Omron Forums Support, -
- 0 replies
- 227 views
To modify a job and create a new product, you Must create the new product first! In Setup mode, go to Advanced settings and click Save Product. By entering a new product name a new copy of the product will be saved. After the new product has been saved, any changes will only be in the new product.
Last reply by Omron Forums Support, -
Problem: Unable to read, no illumination. Targeting if enabled comes on when trigger pulled. Error Message: “No Process Sequence Defined, Please Set the Unit to Default Settings!!” Possible Cause: No Illumination Sequence Define. Solution: Reset Defaults using attached instruction. kA23800000008KBCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 286 views
If you are unable to save bitmap images out of ESP while using the Mobile Hawk, update the firmware to -11 or newer. Firmware is available from the Download Center: http://www.microscan.com/en-us/ServiceAndSupport/DownloadCenter.aspx
Last reply by Omron Forums Support, -
- 0 replies
- 245 views
INTERNAL ONLY. DO NOT MAKE VISIBLE the mounting for the interface pcb in the handle of the Mobile Hawk can break and come loose. The symptoms include a loose cable, and a rattling sound. To test, have the customer wiggle the cable, and see if the connector moves as well.
Last reply by Omron Forums Support, -
- 0 replies
- 187 views
INTERNAL ONLY. If the connector on the Mobile hawk is loose, the interface may have broken loose. Look at the Part Number label and refer to the revision. If Rev. A, the unit probably broke the interface board loose, and should be returned for repair.
Last reply by Omron Forums Support, -
- 0 replies
- 258 views
INTERNAL ONLY. DO NOT PUBLISH. License files are located here: O:\Public_Read\Mfg_Eng\MobileHawkLicenseFiles The data sent by the Mobile Hawk is: License Key Failed!! To restore the Microscan files after a 'Delete all files' or 'U' command - Start the Mobile Hawk - Start ESP - ESP will not see the Mobile Hawk because it is in USB Keyboard mode. Use the button in ESP to set the Mobile Hawk in ESP USB mode. - Load the license file from the Utilities / Firmware / Batch File Upload. The license files can be found at: \\10.10.2.20\vol1\Mfg\Public_Read\Mfg_Eng\MobileHawkLicenseFiles - Power the Mobile Hawk with the trigger button pressed. Repress the button until you hear a bee…
Last reply by Omron Forums Support, -
- 0 replies
- 247 views
This is caused by a missing Mobile Hawk License. To fix this, contact Microscan support 425-203-4841 (helpdesk@microscan.com) with the reader serial number. Provide the serial number, and you will be provided with instructions to continue.
Last reply by Omron Forums Support, -
- 0 replies
- 265 views
MicroHAWK 20 Series Focus displacement from front of window to top of unit is 28.4mm MicroHAWK 30 and 40 Series Focus displacement from front of window to top of unit is 27.9mm Software Version All Firmware Version All Operating System Windows 10
Last reply by Omron Forums Support, -
- 0 replies
- 300 views
Microscan has encountered a situation resulting from a revision level change in a key component of the VS-1 smart camera.The new revision cameras cannot be “downgraded” to operate with older firmware or Visionscape GUIs. For Full Details on The VS-1 Camera Versions and Visionscape Versions please review the attached PDF. kA23800000008EJCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 281 views
The UDP broadcast that the MicroHAWK sends to facilitate its discovery on an Ethernet network uses port 30717. Please ensure that this port stays free on any network where a MicroHAWK might be connected. Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 284 views
To discuss the MicroHAWK PoE implementation and recommended equipment when integrating the device. kA238000000087QCAQ_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 239 views
If after updating the App code some features do not work or it behaves oddly, you need to update the boot code. This is usually only seen if updating an old Microhawk.
Last reply by Omron Forums Support, -
- 0 replies
- 327 views
Below is a table referencing the differences from Hardware Pinout to Parameter naming convention in software. MicroHAWK MV-40 (I/O)PINDescriptionIN/OUTAutoVISIONVisionScape1TriggerINSensorSensor Point12New MasterINDigitalPhysical Input 0001 5Output 1OUTOutput 1Physical Output 000211Output 2OUTOutput 2Physical Output 00036Output 3OUTOutput 3Physical Output 0004 Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 228 views
Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 349 views
Please note that we have had a rash of users complaining that MicroHAWK MV will stop receiving a sensor trigger after a certain period of time. We have traced this to the Debounce time in the camdef. The current solution for this is the give them a modified camdef that sets the Debounce time to 0. Leave the Filter time as is. If you are using AutoVISION only, you will have to edit the original camdef file. In FrontRunner, you can create a copy of the camdef with a modified name and debounce time.
Last reply by Omron Forums Support, -
- 0 replies
- 468 views
Process for Making a MicroHAWK ID reader Dual Boot to MV Update Unit to Latest MicroHAWK ID Version of ID Software 1. Make sure you have the latest version of ESP downloaded and installed on your computer. Unzip to a utility folder for easy access. 2. Make sure you have the latest version of WebLink downloaded to your computer. Unzip to same utility folder for easy access. 3. Upgrade the camera to the latest version of WebLink via ESP. See MicroHAWK Firmware Update Guide in the WebLink file folder for directions. The required files will be in your utility folder. a. Upgrade the App first b. Upgrade WebLink second 4. Rese…
Last reply by Omron Forums Support, -
- 0 replies
- 291 views
In Visionscape FrontRunner Editor, Select the desired Blob tool Click the Show Advanced Datums button Change the Process Every Nth line to 1 The Maximum Blob Size will operate as expected.
Last reply by Omron Forums Support, -
- 0 replies
- 292 views
Below are MFG Part Numbers From Microscan (5M) and TURK versions (10M, 15M, 30M) Common M12-12 pin Plug to M12-12 pin Socket Cordset: Microscan, 61-9000117-01, CORDSET, COMMON, M12 12 PIN PLUG TO M12 12 PIN SOCKET Turck, RKC 12T-10-RSC, M12 12 Pin Plug to 12 Pin Socket – 10M Turck, RKC 12T-15-RSC, M12 12 Pin Plug to 12 Pin Socket – 15M Turck, RKC 12T-30-RSC, M12 12 Pin Plug to 12 Pin Socket – 30M Ethernet M12-8 pin Plug to Standard RJ45 Jack Cordset: Microscan, 61-9000118-01, CORDSET, ETHERNET, M12 8 PIN PLUG TO RJ45, 5M Turck, RSS RJ45S 841-10M, M12 8 PIN PLUG TO RJ45 – 10M Turck, RSS RJ45S 841-15M, M12 8 PIN PLUG TO RJ45 – 15M Turck, RSS RJ45S 841-30M, M12 8 PIN PLUG …
Last reply by Omron Forums Support, -
- 0 replies
- 256 views
Error Message *Windows could not install drivers". For the older Visionscape and DMx AutoID+ hardware keys: http://www3.safenet-inc.com/support/hasp/hasp4/enduser.aspx For the newer GigE Visionscape keys (4.0+), they need the HASP HL drivers: http://www3.safenet-inc.com/support/hasp/enduser.aspx
Last reply by Omron Forums Support, -
- 0 replies
- 286 views
A sample 1 camera equipment list has been created for the I-Pak HE and I-Pak SE configurations I-Pak HE sample equipment list https://na3.salesforce.com/00P500000055XpR I-Pak SE sample equipment list https://na3.salesforce.com/00P500000055XpX
Last reply by Omron Forums Support, -
- 0 replies
- 290 views
The OCV Fontless tool will group touching characters as a single character to be inspected. However if a OCVRuntime or a OCVFont tool is used, a library must be created for each character inspected. This allows the OCVRuntime or OCVFont tool to be able to train a code that has touching characters. Please remember to increase the "Allowed Overlap During Read" found in the LayoutStep datum (tab). For most applications I set this to 5 pixels.
Last reply by Omron Forums Support, -
- 0 replies
- 281 views
During the installation if the CRC error relating to the readme file is displayed. The user can click Ignore and allow the installation to continue. The installation will complete and the I-PAK software will run properly The I-PAK VH error message is shown below Operating System Any
Last reply by Omron Forums Support,